EIM Burst Synchronous Mode in Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

EIM Burst Synchronous Mode in Linux

跳至解决方案
1,768 次查看
jzabalza
Contributor II

Hello

Has anyone used the WEIM Burst Synchronous Mode in Linux?

Some example?

Thanks.

1 解答
1,672 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jose

burst mode can be configured using CSxGCRx EIM registers, in linux dts this is

the timing array "weim-cs-timing"

imx-weim.txt\bus\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

EIM is supported in i.MX6Q Sabre AI board

imx6q-sabreauto-gpmi-weim.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,673 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jose

burst mode can be configured using CSxGCRx EIM registers, in linux dts this is

the timing array "weim-cs-timing"

imx-weim.txt\bus\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

EIM is supported in i.MX6Q Sabre AI board

imx6q-sabreauto-gpmi-weim.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复