EIM Burst Synchronous Mode in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EIM Burst Synchronous Mode in Linux

Jump to solution
1,764 Views
jzabalza
Contributor II

Hello

Has anyone used the WEIM Burst Synchronous Mode in Linux?

Some example?

Thanks.

1 Solution
1,668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jose

burst mode can be configured using CSxGCRx EIM registers, in linux dts this is

the timing array "weim-cs-timing"

imx-weim.txt\bus\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

EIM is supported in i.MX6Q Sabre AI board

imx6q-sabreauto-gpmi-weim.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,669 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jose

burst mode can be configured using CSxGCRx EIM registers, in linux dts this is

the timing array "weim-cs-timing"

imx-weim.txt\bus\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

EIM is supported in i.MX6Q Sabre AI board

imx6q-sabreauto-gpmi-weim.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply