ECSPI2 external HW Loopback test in i.MX8MM EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ECSPI2 external HW Loopback test in i.MX8MM EVK

跳至解决方案
1,556 次查看
sreedhar_appala
Contributor IV

Hi,

I am working with IMX8M Mini EVK and yocto project build details:

 

Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""

I made the dts changes and menuconfig as sugegsted in the thread : test code for checking ECSPI2 on iMX8M Mini EVK 

I want to test the hw loopback : Can I short In the EXP_CN J1003 Pin 19 and Pin 21

pastedImage_2.png

and try running the testcode of SPI using mxc_spi_test1.out.

For testing hw loopback, apart from connecting the J1003 pin 19 and pin 21 together, any other hw care needs to take.

Regards,

Sreedhar

0 项奖励
回复
1 解答
1,486 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, for loopback connecting J1003 pin 19 and pin 21 together
will be sufficient. No additional connections are needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,487 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, for loopback connecting J1003 pin 19 and pin 21 together
will be sufficient. No additional connections are needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,486 次查看
sreedhar_appala
Contributor IV

Thank you Igor.

0 项奖励
回复