ECSPI2 external HW Loopback test in i.MX8MM EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECSPI2 external HW Loopback test in i.MX8MM EVK

ソリューションへジャンプ
1,718件の閲覧回数
sreedhar_appala
Contributor IV

Hi,

I am working with IMX8M Mini EVK and yocto project build details:

 

Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""

I made the dts changes and menuconfig as sugegsted in the thread : test code for checking ECSPI2 on iMX8M Mini EVK 

I want to test the hw loopback : Can I short In the EXP_CN J1003 Pin 19 and Pin 21

pastedImage_2.png

and try running the testcode of SPI using mxc_spi_test1.out.

For testing hw loopback, apart from connecting the J1003 pin 19 and pin 21 together, any other hw care needs to take.

Regards,

Sreedhar

ラベル(3)
0 件の賞賛
返信
1 解決策
1,648件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, for loopback connecting J1003 pin 19 and pin 21 together
will be sufficient. No additional connections are needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,649件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, for loopback connecting J1003 pin 19 and pin 21 together
will be sufficient. No additional connections are needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,648件の閲覧回数
sreedhar_appala
Contributor IV

Thank you Igor.

0 件の賞賛
返信