ECSPI2 external HW Loopback test in i.MX8MM EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECSPI2 external HW Loopback test in i.MX8MM EVK

Jump to solution
1,581 Views
sreedhar_appala
Contributor IV

Hi,

I am working with IMX8M Mini EVK and yocto project build details:

 

Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""

I made the dts changes and menuconfig as sugegsted in the thread : test code for checking ECSPI2 on iMX8M Mini EVK 

I want to test the hw loopback : Can I short In the EXP_CN J1003 Pin 19 and Pin 21

pastedImage_2.png

and try running the testcode of SPI using mxc_spi_test1.out.

For testing hw loopback, apart from connecting the J1003 pin 19 and pin 21 together, any other hw care needs to take.

Regards,

Sreedhar

0 Kudos
Reply
1 Solution
1,511 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, for loopback connecting J1003 pin 19 and pin 21 together
will be sufficient. No additional connections are needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,512 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, for loopback connecting J1003 pin 19 and pin 21 together
will be sufficient. No additional connections are needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,511 Views
sreedhar_appala
Contributor IV

Thank you Igor.

0 Kudos
Reply