Dual parallel camera input!!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual parallel camera input!!!!

2,162件の閲覧回数
chilwonna
Contributor II

Hello,

I want to design with iMX6 dual.

I will connect dual parallel camera.

Cam1 = 1280*720*30fps, YUV ->  IPU#1_CSI0

Cam2 = 2560*1920*30fps, mono Bayer -> IPU#2_CSI1

Display = Parallel display port

Board has to capture two camera at same time and  diplays with Cam1.

Cam2 has to be saved to memory.

Is it possible?

Thanks.

0 件の賞賛
返信
1 返信

1,735件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI chilwonna

in general yes, this may be supported as max. performance is 240MHz per IPU

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------