Dual parallel camera input!!!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dual parallel camera input!!!!

1,570 次查看
chilwonna
Contributor II

Hello,

I want to design with iMX6 dual.

I will connect dual parallel camera.

Cam1 = 1280*720*30fps, YUV ->  IPU#1_CSI0

Cam2 = 2560*1920*30fps, mono Bayer -> IPU#2_CSI1

Display = Parallel display port

Board has to capture two camera at same time and  diplays with Cam1.

Cam2 has to be saved to memory.

Is it possible?

Thanks.

0 项奖励
回复
1 回复

1,143 次查看
igorpadykov
NXP Employee
NXP Employee

HI chilwonna

in general yes, this may be supported as max. performance is 240MHz per IPU

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------