Hi,
We have LVDS and HDMI display connected to imx6 board and both displays are showing mirrored contents.
But when i query , its always returning display count as 1.
---------------------------------------------------------------------------------------------------------------
DisplayManager manager = (DisplayManager) getSystemService(DISPLAY_SERVICE);
 Display[] displays = manager.getDisplays(DisplayManager.DISPLAY_CATEGORY_PRESENTATION);
 Log.w("Display", "Display No = " + displays.length);
---------------------------------------------------------------------------------------------------------------
Why the display count is not shown as 2, since we have HDMI and LVDS connected ?
Solved! Go to Solution.
 
					
				
		
 Rita_Wang
		
			Rita_Wang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
I have confirmed it for you, that the default BSP can not support your above requirement. You want the HDMI and LVDS screen display different conten, here you need do BSP modify. I can send you the patch for i.MX6 Triple Display application. You can refer to and follow the document and patch. The files are large, here I share it with you bellow.
Link: http://pan.baidu.com/s/1nuLC30l Password: au72
Have a great day,
 Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
After enabling - "Android Settings à Developer Options à Drawing à Simulate secondary displays" , the display count is incremented.
New screens are coming on the same display(HDMI) as overlay. We want the new screens to be shown in different display(LVDS).
Any suggestions on what to be done ?
 
					
				
		
 Rita_Wang
		
			Rita_Wang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
In the android BSP, it default support the dual display LVDS and HDMI. If the first display is LVDS, The HDMI as second display, the content on the HDMI screen is scale content from LVDS.
Have a great day,
 Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
Thank you for the reply.
We want to run one application on HDMI and another application on LVDS (not same content), is it possible on Android BSP ?
If yes could you please direct us.
Our board : iMX6Q SABRE AI CPU + Base Borad
 
					
				
		
 Rita_Wang
		
			Rita_Wang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
I have confirmed it for you, that the default BSP can not support your above requirement. You want the HDMI and LVDS screen display different conten, here you need do BSP modify. I can send you the patch for i.MX6 Triple Display application. You can refer to and follow the document and patch. The files are large, here I share it with you bellow.
Link: http://pan.baidu.com/s/1nuLC30l Password: au72
Have a great day,
 Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is there Android 7.1 patches released?
 
					
				
		
I have successfully applied all the patches except one from "i.MX6DQP_Android_M_6.0.1_TripleDisplay_Beta".
Could you please help me on resolving this ?
Error Log :
-------------------------------------------------------------------------------------------------------------
root@ubuntu:/home/developer/myandroid/device/fsl-proprietary# git am 0001-Triple-Display.patch 
Applying: Triple Display
error: the patch applies to 'fsl-hwc/hwcomposer_fsl.imx6.so' (37862f399c36c6ade3683edebbc54f6d749d4f69), which does not match the current contents.
error: fsl-hwc/hwcomposer_fsl.imx6.so: patch does not apply
Patch failed at 0001 Triple Display
The copy of the patch that failed is found in:
 /home/developer/myandroid/device/fsl-proprietary/.git/rebase-apply/patch
When you have resolved this problem, run "git am --continue".
If you prefer to skip this patch, run "git am --skip" instead.
To restore the original branch and stop patching, run "git am --abort".
-------------------------------------------------------------------------------------------------------------
 
					
				
		
I am able to successfully show different contents on both HDMI and LVDS screen.
But I am loosing the touch capability on HDMI while showing different contents and i need a mouse to continue work.
If the contents are same on both screens then this issue is not present.
As I have mentioned above , I was unable to apply one patch "root@ubuntu:/home/developer/myandroid/device/fsl-proprietary# git am 0001-Triple-Display.patch".
If this can cause the issue then could you please provide the "fsl-hwc/hwcomposer_fsl.imx6.so".
Else please guide me on this issue.
Thanks,
Kiran
Did you solve the problem you mentioned above . I have met the same issue .
error: the patch applies to 'fsl-hwc/hwcomposer_fsl.imx6.so' (37862f399c36c6ade3683edebbc54f6d749d4f69), which does not match the current contents.
error: fsl-hwc/hwcomposer_fsl.imx6.so: patch does not apply
 
					
				
		
No , I could not resolve this issue.
I did asked this as a separate thread in Touch not working on i.MX6 Android Dual display.
Waiting for the reply.
 
					
				
		
Thank you for the confirmation and the patch.
I will check the patch and come back.
Thank you,
Kiran
 
					
				
		
 Rita_Wang
		
			Rita_Wang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Are you using the MCIMX6QAICPU board?
Have a nice day
Rita
 
					
				
		
Our board : iMX6Q SABRE AI CPU + Base Borad