Question, ERR011115 of i.MX6UltraLite errata

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, ERR011115 of i.MX6UltraLite errata

2,984 Views
SLICE
Contributor IV

Dear team,

My customer is using i.MX6SoloLite now. And they found ER011115, boot failure, have been added to errata document of i.MX6UltraLite.

The customer has a concern whether if this erratum, ER011115, can affect to i.MX6SoloLite also.

Is the ER011115 specific to i.MX6UltraLite? No need to have such concern on i.MX6SoloLite?

Thanks,

Miyamoto

Labels (2)
0 Kudos
1 Reply

334 Views
Yuri
NXP Employee
NXP Employee

Hello,

 ERR011115 (System Boot: Boot failures on certain devices when the boot
image targets OCRAM) takes place only for i.MX 6UltraLite silicon revision
1.2 device, shipped prior to date code 1740.

   IMX6 SL is not affected.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos