Dual display functionality support on custom board based on iMX6 running Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dual display functionality support on custom board based on iMX6 running Yocto

2,872 次查看
alexeylugovskoy
Contributor II

Hello, Everyone!

1. System description:

We are using a custom boards with iMX6Solo and iMX6Quad processors from different h/w vendors. The requirement is to bring up dual display functionality on these boards. We use standard Yocto 2.2 with layer meta-fsl-arm from git.yoctoproject.org/meta-fsl-arm and Wayland/Weston graphics packages. Weston backend uses fbdev.

Additional Weston command line options for running graphics in dual display configuration are the following:

weston --tty=1 --use-gal2d --device=/dev/fb0,/dev/fb2

Packet version:

imx-gpu-viv_5.0.11.p4.5

Kernels:

4.1.15

3.14.28

2. Problem description

 We tried to bring up dual display functionality on h/w boards and configurations described above. For all configurations we observe the the same issue - on a first display (no matter it's HDMI or LVDS/LCD) graphics work in a proper way without glitches and blinks; on a second display we always observe blinks and glitches/artifacts on open windows during cursor movement and input events. This can be reproduced with 32/16 bpp and does not depend on resolution. 

We can't determine the root cause of this problem. Has anyone successfully brought up dual display configuration using iMX6 Yocto with imx-gpu-viv_5.0.11.p4.5? Any suggestions how to workaround the issue described above?

Thanks in advance!

Alexey

0 项奖励
回复
4 回复数

2,019 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

L3.14.52 has a known issue where the fbGetDisplay function called by the fbdev compositor on weston does not return a different display index, thus not being able to render on multiple screens at a time, You need to use the latest fsl_5.0.11.p4.7 Libraries to solve it.

 

GitHub - Freescale/kernel-module-imx-gpu-viv: FSL Community fork of Vivante i.MX GPU Linux kernel dr...

 

regards

2,019 次查看
alexeylugovskoy
Contributor II

Hello,

Many thanks for your feedback! Could you please clarify what version of Weston is used for mentionded imx-gpu-viv 5.0.11 8.6? The latests one seems still have issues described above. There is Weston fork to include support for Freescale i.MX (https://github.com/Freescale/weston-imx), but it's quite old and is not compatible with libinput from yocto 2.x.

Thanks,

Alexey

0 项奖励
回复

2,019 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Please check the pacthes for weston 1.9 and Latest BSP based on 4.1.5 with gpu p8.3

https://community.nxp.com/thread/391972 

regards

2,019 次查看
alexeylugovskoy
Contributor II

Thanks! I found that similar issue has been discussed here:

https://community.nxp.com/thread/443216 

0 项奖励
回复