Dual die DDR support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,139件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Let me confirm about DDR support.

I plan to use H5TC8G63CMR and think it can use dual die device without concern.

Can i.MX6SL support dual die DDR device ?

if yes, is there any concern (ex. it cannot use when booting.)?

Ko-hey

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,039件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

H5TC8G63CMR will work fine with i.MX6SL.

No concerns.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,040件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

H5TC8G63CMR will work fine with i.MX6SL.

No concerns.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,039件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thank you !

ko-hey

0 件の賞賛
返信