Dual die DDR support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual die DDR support

Jump to solution
2,152 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about DDR support.

I plan to use H5TC8G63CMR and think it can use dual die device without concern.

Can i.MX6SL support dual die DDR device ?

if yes, is there any concern (ex. it cannot use when booting.)?

Ko-hey

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
2,052 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

H5TC8G63CMR will work fine with i.MX6SL.

No concerns.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,053 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

H5TC8G63CMR will work fine with i.MX6SL.

No concerns.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,052 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you !

ko-hey

0 Kudos
Reply