Dual Parallel Camera, I.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Parallel Camera, I.MX6

Jump to solution
2,129 Views
JHY
Contributor IV

Is it possible to recieve 2ch, 720p@30fps, BT.656, 4:2:2 format, 54MHz, each CSI port of I.MX6DUAL?

I think it can because there are two IPU units.

what do you think, experts?

v.jpg

Labels (2)
0 Kudos
Reply
1 Solution
1,927 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically up to three cameras may be connected to the i.MX6 D/Q.

Please refer to Figure 9-3.(The Video Input Ports) of the i.MX6 D/Q RM.

  According to section 9.2.1.1 (Camera Ports) :

"The input rate supported by the camera port is as follows:

• Peak: up to 240 MHz (values/sec)

• Average (assuming 35% blanking overhead), for YUV 4:2:2

• Pixel in one cycle (e.g. BT.1120): up to 180 MP/sec, e.g. 12M pixels @ 15 fps

• Pixel on two cycles (e.g. BT.656): up to 90 MP/sec, e.g. 6M pixels @ 15 fps."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,928 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically up to three cameras may be connected to the i.MX6 D/Q.

Please refer to Figure 9-3.(The Video Input Ports) of the i.MX6 D/Q RM.

  According to section 9.2.1.1 (Camera Ports) :

"The input rate supported by the camera port is as follows:

• Peak: up to 240 MHz (values/sec)

• Average (assuming 35% blanking overhead), for YUV 4:2:2

• Pixel in one cycle (e.g. BT.1120): up to 180 MP/sec, e.g. 12M pixels @ 15 fps

• Pixel on two cycles (e.g. BT.656): up to 90 MP/sec, e.g. 6M pixels @ 15 fps."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply