Dual Parallel Camera, I.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dual Parallel Camera, I.MX6

跳至解决方案
1,409 次查看
JHY
Contributor IV

Is it possible to recieve 2ch, 720p@30fps, BT.656, 4:2:2 format, 54MHz, each CSI port of I.MX6DUAL?

I think it can because there are two IPU units.

what do you think, experts?

v.jpg

标签 (2)
0 项奖励
回复
1 解答
1,207 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Basically up to three cameras may be connected to the i.MX6 D/Q.

Please refer to Figure 9-3.(The Video Input Ports) of the i.MX6 D/Q RM.

  According to section 9.2.1.1 (Camera Ports) :

"The input rate supported by the camera port is as follows:

• Peak: up to 240 MHz (values/sec)

• Average (assuming 35% blanking overhead), for YUV 4:2:2

• Pixel in one cycle (e.g. BT.1120): up to 180 MP/sec, e.g. 12M pixels @ 15 fps

• Pixel on two cycles (e.g. BT.656): up to 90 MP/sec, e.g. 6M pixels @ 15 fps."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,208 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Basically up to three cameras may be connected to the i.MX6 D/Q.

Please refer to Figure 9-3.(The Video Input Ports) of the i.MX6 D/Q RM.

  According to section 9.2.1.1 (Camera Ports) :

"The input rate supported by the camera port is as follows:

• Peak: up to 240 MHz (values/sec)

• Average (assuming 35% blanking overhead), for YUV 4:2:2

• Pixel in one cycle (e.g. BT.1120): up to 180 MP/sec, e.g. 12M pixels @ 15 fps

• Pixel on two cycles (e.g. BT.656): up to 90 MP/sec, e.g. 6M pixels @ 15 fps."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复