Dual Parallel Camera, I.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual Parallel Camera, I.MX6

ソリューションへジャンプ
2,118件の閲覧回数
JHY
Contributor IV

Is it possible to recieve 2ch, 720p@30fps, BT.656, 4:2:2 format, 54MHz, each CSI port of I.MX6DUAL?

I think it can because there are two IPU units.

what do you think, experts?

v.jpg

ラベル(2)
0 件の賞賛
返信
1 解決策
1,916件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Basically up to three cameras may be connected to the i.MX6 D/Q.

Please refer to Figure 9-3.(The Video Input Ports) of the i.MX6 D/Q RM.

  According to section 9.2.1.1 (Camera Ports) :

"The input rate supported by the camera port is as follows:

• Peak: up to 240 MHz (values/sec)

• Average (assuming 35% blanking overhead), for YUV 4:2:2

• Pixel in one cycle (e.g. BT.1120): up to 180 MP/sec, e.g. 12M pixels @ 15 fps

• Pixel on two cycles (e.g. BT.656): up to 90 MP/sec, e.g. 6M pixels @ 15 fps."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,917件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Basically up to three cameras may be connected to the i.MX6 D/Q.

Please refer to Figure 9-3.(The Video Input Ports) of the i.MX6 D/Q RM.

  According to section 9.2.1.1 (Camera Ports) :

"The input rate supported by the camera port is as follows:

• Peak: up to 240 MHz (values/sec)

• Average (assuming 35% blanking overhead), for YUV 4:2:2

• Pixel in one cycle (e.g. BT.1120): up to 180 MP/sec, e.g. 12M pixels @ 15 fps

• Pixel on two cycles (e.g. BT.656): up to 90 MP/sec, e.g. 6M pixels @ 15 fps."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信