Does i.MX6 quad core processor support eMMC 5.0 HS400 interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does i.MX6 quad core processor support eMMC 5.0 HS400 interface

2,393 次查看
harishnaidu
Contributor II

Does i.MX6 quad core processor support eMMC 5.0 HS400 interface

标签 (2)
2 回复数

1,524 次查看
justin_jiang
NXP Employee
NXP Employee

Compatible with the MMC System Specification version 4.2/4.3/4.4, no eMMC 5.0 support.

1,524 次查看
gusarambula
NXP TechSupport
NXP TechSupport

The i.MX6Q external memory controller supports eMMC up to rev 4.4/4.41. You may find more information on the i.MX6Q Data Sheet (link below).

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Unfortunately eMMC 5.0 is not supported (along with the HS400 interface which was introduced in this eMMC revision).