Does i.MX6 quad core processor support eMMC 5.0 HS400 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX6 quad core processor support eMMC 5.0 HS400 interface

3,095件の閲覧回数
harishnaidu
Contributor II

Does i.MX6 quad core processor support eMMC 5.0 HS400 interface

ラベル(2)
2 返答(返信)

2,226件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Compatible with the MMC System Specification version 4.2/4.3/4.4, no eMMC 5.0 support.

2,226件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

The i.MX6Q external memory controller supports eMMC up to rev 4.4/4.41. You may find more information on the i.MX6Q Data Sheet (link below).

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Unfortunately eMMC 5.0 is not supported (along with the HS400 interface which was introduced in this eMMC revision).