Does NXP i.MX6ULL SDK support Debian?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does NXP i.MX6ULL SDK support Debian?

2,028件の閲覧回数
jupiter_hce
Contributor III

It seems that NXP SDK developed its own Linux Yocto, but I am interested in using Debian, anyone knows if NXP SDK supports Debian for i.MX6ULL or not?

Thank you

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,769件の閲覧回数
linda_zhang
Contributor IV

We are using MYIR's MYS-6ULX board, it Supports Linux with Debian distribution or by Yocto Project with ported QT. The board comes with yocto by default.

MYS-6ULX | NXP i.MX 6UltraLite, 6ull, IoT, IND, ARM Cortex-A7, Linux, Debian, Yocto, Single Board Co... 

0 件の賞賛
返信

1,769件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you are referring to the SDK package for i.MX6ULL, it could be installed on Windows, and on Linux versions with support for the toolchain (GCC), and the downloadable code for i.MX is running bare-metal or FreeRTOS.

If you are referring to the BSPs available for the i.MX6ULL, they are Linux, built on Yocto project.

Debian or other Linux distribution could run on i.MX processors, but they are not released nor supported by NXP. You could take a look at the following Community documents with such kind of implementations, just for reference:

https://community.nxp.com/docs/DOC-330147

https://community.nxp.com/docs/DOC-328362


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信