Document problem about iMX6 Android patches

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Document problem about iMX6 Android patches

Jump to solution
4,258 Views
DeanHuang
Contributor III

Hi,

I have a imx6 android question.

In Android User Guide, writes:

Get R13.4-GA kernel source code from freescale's opensource git:

$ cd myandroid

$ git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx # the kernel repo is

heavy, so this can take a while

$ cd kernel_imx

$ git checkout imx-android-13.4.1


Does it mean that I do not need to do this in "Patch code for i.MX"

Assume you had unzipped i.MX Android release package to /opt/imx-android-13.4.1/.

$ cd ~/myandroid

$ source /opt/imx-android-13.4.1/code/13.4.1/and_patch.sh

$ help

Now you should see that the "c_patch" function is available

$ c_patch /opt/imx-android-13.4.1/code/13.4.1 imx_13.4.1


I just need to do this ?

If your software has upgraded to R13.4-GA and you would only like to apply the additional patches between R13.4-GA and

13.4.1, please use the following steps:

Take framwork/base.git as an example. Assume you had unzipped i.MX Android release package

to /opt/imx-android-13.4.1/ .

$ cd /opt/imx-android-13.4.1/code/13.4.1-delta/platform/frameworks/base.git

$ ls *.patch > series

$ cd ~/myandroid/frameworks/base

$ git quiltimport --patches /opt/imx-android-13.4.1/code/13.4.1-delta/platform/frameworks/

base.git

I just have some confuse.

Thanks!!

Labels (2)
1 Solution
2,826 Views
DeanHuang
Contributor III

Dears,

I had solved this problem. It should use "imx-android-13.4.1/code/13.4.1/" instead of "imx-android-13.4.1/code/13.4.1-delta".

But I still have one question:

When I compiling the source code, there are some error messages.

ex:

host C++: obbtool <= frameworks/base/tools/obbtool/Main.cpp
:0:0: error: “_FORTIFY_SOURCE” redefined [-Werror]
:0:0: note: this is the location of the previous definition
cc1plus: all warnings being treated as errors


or

ERROR:  frameworks/compile/slang/slang_rs_export_foreach.cpp:247:23:
error: variable ‘ParamName’ set but not used [-Werror=unused-but-set- variable]


I had building image successfully  by correcting source code. But I'm confused that these error are source code problem or compiling environment problem?

My environment is Ubuntu 12.04 64 bit.

View solution in original post

0 Kudos
Reply
3 Replies
2,827 Views
DeanHuang
Contributor III

Dears,

I had solved this problem. It should use "imx-android-13.4.1/code/13.4.1/" instead of "imx-android-13.4.1/code/13.4.1-delta".

But I still have one question:

When I compiling the source code, there are some error messages.

ex:

host C++: obbtool <= frameworks/base/tools/obbtool/Main.cpp
:0:0: error: “_FORTIFY_SOURCE” redefined [-Werror]
:0:0: note: this is the location of the previous definition
cc1plus: all warnings being treated as errors


or

ERROR:  frameworks/compile/slang/slang_rs_export_foreach.cpp:247:23:
error: variable ‘ParamName’ set but not used [-Werror=unused-but-set- variable]


I had building image successfully  by correcting source code. But I'm confused that these error are source code problem or compiling environment problem?

My environment is Ubuntu 12.04 64 bit.

0 Kudos
Reply
2,826 Views
LeonardoSandova
Specialist I

Hi Dean, it would be great if you post the patch with all the changes needed to compile android on your Ubuntu machine. About your question, I am not sure, but it may be the host system your are using to compile Android.

0 Kudos
Reply
2,826 Views
DeanHuang
Contributor III

Hi Leonardo,

These are the error messages and solutions I found from network. There may be other solutions.

My Environment:

Ubuntu 12.04 64 bit

imx-android-13.4.1.tar.gz

Sorry for that I forget what ubuntu packages I installed before building Android.

Q1

host C++: obbtool <= frameworks/base/tools/obbtool/Main.cpp
     :0:0: error: “_FORTIFY_SOURCE” redefined [-Werror]
     :0:0: note: this is the location of the previous definition
     cc1plus: all warnings being treated as errors

S1

To fix this, edit build/core/combo/HOST_linux-x86.mk and replace:
     HOST_GLOBAL_CFLAGS += -D_FORTIFY_SOURCE=0
with
     HOST_GLOBAL_CFLAGS += -U_FORTIFY_SOURCE -D_FORTIFY_SOURCE=0


Q2

ERROR:  frameworks/compile/slang/slang_rs_export_foreach.cpp:247:23:
error: variable ‘ParamName’ set but not used [-Werror=unused-but-set-
variable]

S2

android/ics/frameworks/compile/slang/Android.mk
-local_cflags_for_slang := -Wno-sign-promo -Wall -Wno-unused-parameter -Werror
+local_cflags_for_slang := -Wno-sign-promo -Wall -Wno-unused-parameter


Q3

external/mesa3d/src/glsl/linker.cpp: In function ‘void link_shaders(const gl_context*, gl_shader_program*)’:
external/mesa3d/src/glsl/linker.cpp:1734:49: error: expected primary-expression before ‘,’ token
external/mesa3d/src/glsl/linker.cpp:1734:50: error: ‘fragColor’ was not declared in this scope
external/mesa3d/src/glsl/linker.cpp:1734:59: error: ‘offsetof’ was not declared in this scope
make: *** [out/host/linux-x86/obj/STATIC_LIBRARIES/libMesa_intermediates/src/glsl/linker.o] Error 1

S3

Adding a "#include <stddef.h>" to linker.cpp


Q4

ERROR:  external/oprofile/libpp/format_output.h:94:22: error:
reference ‘counts’ cannot be declared ‘mutable’ [-fpermissive]

S4

external/oprofile/libpp/format_output.h
-               mutable counts_t & counts;
+               counts_t & counts;


Q5

android_repo/external/llvm/lib/Support/Mutex.cpp:69: undefined reference to `pthread_mutexattr_init'
android_repo/external/llvm/lib/Support/Mutex.cpp:75: undefined reference to `pthread_mutexattr_settype'
android_repo/external/llvm/lib/Support/Mutex.cpp:80: undefined reference to `pthread_mutexattr_setpshared'
android_repo/external/llvm/lib/Support/Mutex.cpp:89: undefined reference to `pthread_mutexattr_destroy'
out/host/linux-x86/obj/STATIC_LIBRARIES/libLLVMSupport_intermediates/libLLVMSupport.a(Mutex.o): In function `llvm::sys::MutexImpl::tryacquire()':
android_repo/external/llvm/lib/Support/Mutex.cpp:143: undefined reference to `pthread_mutex_trylock'
collect2: ld returned 1 exit status

S5

Way1:
system/extras/tests/bionic/libc/Android.mk
LOCAL_MODULE_TAGS := tests

-LOCAL_LDFLAGS := \
+LOCAL_LDLIBS := \
    -lpthread \
    -ldl

Way2:
external/llvm/llvm-host-build.mk
LOCAL_LDLIBS := -lpthread -ldl


Q6

external/gtest/src/../src/gtest-filepath.cc:180:28: warning: missing initializer for member ‘stat::st_dev’ [-Wmissing-field-initializers]

external/gtest/src/../src/gtest-filepath.cc:180:28: warning: missing initializer for member ‘stat::__pad1’ [-Wmissing-field-initializers]

...
...
...
external/gtest/src/../src/gtest-filepath.cc:208:28: warning: missing initializer for member ‘stat::st_ino’ [-Wmissing-field-initializers]
make: *** [out/host/linux-x86/obj/STATIC_LIBRARIES/libgtest_host_intermediates/gtest-all.o] Error 1

S6

external/gtest/include/gtest/internal/gtest-param-util.h
add
#include <cstddef>