Android factory reset on i.Mx. 6 SoloLite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android factory reset on i.Mx. 6 SoloLite

1,247件の閲覧回数
kf5obs
Contributor I

Community,

how can I perform a factory reset on the Android? I must have messed up the Android somehow. When I apply power to the SoloLite kit, the Android logo appears and after few seconds there's a flicker (logo appears) and the logo re-appears. It seems like I broke the android somehow. Is there an easy way to reset the android? Is there a recovery mode I can enter with keyboard commands or will I need the serial interface?

ラベル(2)
0 件の賞賛
返信
1 返信

1,089件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Most probably you will need to flash the SD Card to a clean Android installation, but can you to a serial terminal connection and let me know where it stalls/loops/errors out?