Display Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Display Support

1,950件の閲覧回数
abhinandansingh
Contributor I

Hi 

I am using IMx6 Quad processor . 

I want to drive two outputs to support two displays.

Outputs are : 

  • VGA
  • DisplayPort

Inputs are :

  • LVDS 1 Port: 170 Mpixels/Sec or LVDS x 2 ports: 85 Mpixels/sec
  • HDMI 1.4 a
  • RGB 24 Bit 266 Mpixels/sec

Resolution : 1920 x 1080 @ 60 Hz.

Please recommend an approach on how can I simultaneously drive both displays via VGA and a DisplayPort .

I believe single LVDS cannot support such HD resolution and thus I will be needing to use 2 LVDS for it. 

Still, anyone giving any leads will be highly appreciated. 

Thanks

0 件の賞賛
返信
1 返信

1,893件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell me which version of BSP are you using?

0 件の賞賛
返信