Hello
boot:dhcp:
From ifconfig, both interfaces have same MAC addresses, but no IP addresses although the interfaces are configured for
DHCP:
The status LEDs on the ethernet ports are not even on.
Any thoughts on how to fix this issue?
try to use "ifconfig eth0 address" to set the eth0 ip address, then in the uboot, use "setenv serverip address" this adress is same as eth0
Thank you for your advice!
Follow the method you provided,then in the uboot,"setenv ipaddr 192.168.1.59",But after entering the Linux, there is still no IP address.
The final question is that the eht0 and eth1 is not link.The status LEDs on the ethernet ports are not even on
I mentioned that you need to set the same serverip as eth0, not ipaddr