Display Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display Support

1,959 Views
abhinandansingh
Contributor I

Hi 

I am using IMx6 Quad processor . 

I want to drive two outputs to support two displays.

Outputs are : 

  • VGA
  • DisplayPort

Inputs are :

  • LVDS 1 Port: 170 Mpixels/Sec or LVDS x 2 ports: 85 Mpixels/sec
  • HDMI 1.4 a
  • RGB 24 Bit 266 Mpixels/sec

Resolution : 1920 x 1080 @ 60 Hz.

Please recommend an approach on how can I simultaneously drive both displays via VGA and a DisplayPort .

I believe single LVDS cannot support such HD resolution and thus I will be needing to use 2 LVDS for it. 

Still, anyone giving any leads will be highly appreciated. 

Thanks

0 Kudos
Reply
1 Reply

1,902 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell me which version of BSP are you using?

0 Kudos
Reply