Disabling JTAG on IMX7d

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disabling JTAG on IMX7d

ソリューションへジャンプ
3,083件の閲覧回数
stephendonn
Contributor I

Hi

I'm trying to disable JTAG on an IMX7d. IMX7DSSRM refers to eFuse SJC_DISABLE, but I can't seem to find which OCOTP fuse this is. Is there release note or some such similar to AN4686 for the IMX7d?

Kind regards

Steve

ラベル(1)
1 解決策
2,872件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Table 6-19 in ref. manual shows that it is bit 21 at 0x470 fuse address. Looking at OCOTP chapter, that would be OTP Bank 1, Word 3 (OCOTP_BOOT_CFG0).

元の投稿で解決策を見る

3 返答(返信)
2,872件の閲覧回数
stephendonn
Contributor I

Thank you for the information. 

0 件の賞賛
返信
2,873件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Table 6-19 in ref. manual shows that it is bit 21 at 0x470 fuse address. Looking at OCOTP chapter, that would be OTP Bank 1, Word 3 (OCOTP_BOOT_CFG0).

2,872件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Steve

this fuse is described in sect.6.3.1 Boot Fusemap i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Fuse programming:

https://community.nxp.com/docs/DOC-95458 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------