Digital silicon Microphone with I2S interface connect to I.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Digital silicon Microphone with I2S interface connect to I.MX6ULL

Jump to solution
2,032 Views
KuiLu
Contributor I

I  have 2 I2S digital microphone with I2S interface,

KuiLu_0-1644288819405.png

 

The connection with iMX6ULL will be:

I2S_CLK -> CSI_DATA05 -> SAI1_TX_BCLK;

I2S_WS -> CSI_DATA04 -> SAI1_TX_SYNC;

I2S_DATA -> CSI_DATA06 -> SAI1_RX_DATA;

Will this correct?

If this pads config to ESAI, will be worked also?

0 Kudos
Reply
1 Solution
1,958 Views
art
NXP Employee
NXP Employee

Yes, the microphone connection schematic you show and i.MX6ULL pin assignment are correct.

Best Regards,
Artur

View solution in original post

0 Kudos
Reply
2 Replies
1,959 Views
art
NXP Employee
NXP Employee

Yes, the microphone connection schematic you show and i.MX6ULL pin assignment are correct.

Best Regards,
Artur

0 Kudos
Reply
1,949 Views
KuiLu
Contributor I

Artur, thanks. Lu Kui

0 Kudos
Reply