Digital silicon Microphone with I2S interface connect to I.MX6ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Digital silicon Microphone with I2S interface connect to I.MX6ULL

跳至解决方案
1,683 次查看
KuiLu
Contributor I

I  have 2 I2S digital microphone with I2S interface,

KuiLu_0-1644288819405.png

 

The connection with iMX6ULL will be:

I2S_CLK -> CSI_DATA05 -> SAI1_TX_BCLK;

I2S_WS -> CSI_DATA04 -> SAI1_TX_SYNC;

I2S_DATA -> CSI_DATA06 -> SAI1_RX_DATA;

Will this correct?

If this pads config to ESAI, will be worked also?

0 项奖励
回复
1 解答
1,609 次查看
art
NXP Employee
NXP Employee

Yes, the microphone connection schematic you show and i.MX6ULL pin assignment are correct.

Best Regards,
Artur

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,610 次查看
art
NXP Employee
NXP Employee

Yes, the microphone connection schematic you show and i.MX6ULL pin assignment are correct.

Best Regards,
Artur

0 项奖励
回复
1,600 次查看
KuiLu
Contributor I

Artur, thanks. Lu Kui

0 项奖励
回复