Hello, when I make changes to my evk board dts file, the changes don’t seem to make it to the image. To generate the image, I follow the standard procedure listed in IMXLXYOCTOUG and here is how I make the changes to my dts file:
bitbake virtual/kernel
bitbake -c devshell virtual/kernel
This opens a new shell. I make changes to imx8mn_evk.dts within tmp/work-shared/… directory and I then compile dts files within the new shell.
make dtbs
I exit the shell and then issue:
bitbake -c deploy virtual/kernel
Is this the correct procedure to update the board dts file? I am not sure if I am updating the correct file location or if I need to copy the file? Any guidance on how I should do this and why isn’t it working that would be appreciated. Thank you!
解決済! 解決策の投稿を見る。
Sure. Say I wanted to modify the devtree for an imx8m nano (ddr4 version):
I source my setup script into the build directory then:
I've been using devtool to make changes to the device trees.
@amberworth any chance you could provide more details or instructions? I have used devtool to create/modify/upgrade a recipe but not sure how to use it to modify and update a devicetree file. Thank you!
Sure. Say I wanted to modify the devtree for an imx8m nano (ddr4 version):
I source my setup script into the build directory then:
Thank you @amberworth for the detailed instructions. This actually worked just fine. I was also able to get it working using the devshell method. I found this link to be useful https://stackoverflow.com/questions/34175786/how-to-install-kernel-patch-locally-in-yocto/34187967
Thanks!