DDR4 4GB Interface btw 8MQ and 2x 2GB 16b DDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR4 4GB Interface btw 8MQ and 2x 2GB 16b DDR4

3,251件の閲覧回数
Jack-Cha
Contributor V

Hi i.MX 8M Champs

Could you please help to expain about DDR4 interface regarding the Max 4GB ( 2x 2GB ) size support?

A customer would use Micron DDR4, MT40A1G16TB-062EF.

They're unable to pass the stress test yet. Hence we're under support to figure out the cause of failure.

We'd like to check if 2x DDR4 have the appropriate connection with 8MQ.

Jacky7_0-1695785875933.png

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

3,225件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I see that the cs pin you do not connect to cpu side in your design, you need to connect to cs0 of the i.MX8MQ.
You can check it.

0 件の賞賛
返信

3,209件の閲覧回数
Jack-Cha
Contributor V

Hi 

Thanks for your kind reply.

They used CS0 for both DDR1 and DDR2 as below.

Also attched pdf.

Jacky7_0-1695826771415.png

Jacky7_1-1695826817275.png

Jacky7_2-1695826833894.png

 

 

 

 

0 件の賞賛
返信

3,230件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you share us the cpu side picture to us, it is not clear?

0 件の賞賛
返信

3,167件の閲覧回数
Jack-Cha
Contributor V

Hi 

CPU side is also included in attached DDR page.pdf from above post.

Thanks.

Regards, 

Jack

0 件の賞賛
返信