DDR3L SDRAM interface with iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3L SDRAM interface with iMX6

2,508 Views
mrudangshelat
Contributor IV

Hi, I am using DDR3L SDRAM with 32 bit interface with iMX6 in my design. iMX6 has 64bit data capacity. If i am using only 32 bit channel 0, so do i need to keep NC channel1 or is there any specific connections/level i need to do in my design. Thanks, Mrudang

Labels (1)
0 Kudos
Reply
8 Replies

2,152 Views
Yuri
NXP Employee
NXP Employee

Hello,

Unused signals / pins of 64-bit memory I/F (in 32-bit or 16-bit mode) may be left float,
as stated in section 5 (DRAM interface requirements for migration) of app note AN4397

(Common Hardware Design for i.MX  6Dual/6Quad and i.MX 6Solo/6DualLite).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,152 Views
mrudangshelat
Contributor IV

Hi Yuri,

Thanks for reply.

I have attached my design, can you please review it and provide me feedback.

I have added 2 files (16bit and 32bit design)

Thanks & regards,

Mrudang

DDR3L - iMX6 Interface - 16bit.jpg

DDR3L - iMX6 Interface - 32bit.jpg

0 Kudos
Reply

2,152 Views
Yuri
NXP Employee
NXP Employee

Hi,

Quality of the figures is not good. Please create request and provide original scheme
sheets.

How to submit a new question for NXP Support

Regards,

Yuri.

0 Kudos
Reply

2,152 Views
mrudangshelat
Contributor IV

Hi Yuri,

Thanks for prompt support.

I have tried to open new request but due to some issue it's not accepting my User name and password.

Could you please provide me your email address or alternate contact details, so I can send you PDF file for review.

And I am also not able to attach PDF design file with this message.

Thanks & regards,

Mrudang

0 Kudos
Reply

2,152 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply

2,152 Views
mrudangshelat
Contributor IV

Thanks Yuri.

0 Kudos
Reply

2,152 Views
Yuri
NXP Employee
NXP Employee

I send comments via e-mail.

~Yuri.

0 Kudos
Reply

2,152 Views
mrudangshelat
Contributor IV

Thanks Yuri,

For your valuable feedback.

0 Kudos
Reply