DDR3L SDRAM interface with iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3L SDRAM interface with iMX6

2,493件の閲覧回数
mrudangshelat
Contributor IV

Hi, I am using DDR3L SDRAM with 32 bit interface with iMX6 in my design. iMX6 has 64bit data capacity. If i am using only 32 bit channel 0, so do i need to keep NC channel1 or is there any specific connections/level i need to do in my design. Thanks, Mrudang

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

2,137件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Unused signals / pins of 64-bit memory I/F (in 32-bit or 16-bit mode) may be left float,
as stated in section 5 (DRAM interface requirements for migration) of app note AN4397

(Common Hardware Design for i.MX  6Dual/6Quad and i.MX 6Solo/6DualLite).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,137件の閲覧回数
mrudangshelat
Contributor IV

Hi Yuri,

Thanks for reply.

I have attached my design, can you please review it and provide me feedback.

I have added 2 files (16bit and 32bit design)

Thanks & regards,

Mrudang

DDR3L - iMX6 Interface - 16bit.jpg

DDR3L - iMX6 Interface - 32bit.jpg

0 件の賞賛
返信

2,137件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

Quality of the figures is not good. Please create request and provide original scheme
sheets.

How to submit a new question for NXP Support

Regards,

Yuri.

0 件の賞賛
返信

2,137件の閲覧回数
mrudangshelat
Contributor IV

Hi Yuri,

Thanks for prompt support.

I have tried to open new request but due to some issue it's not accepting my User name and password.

Could you please provide me your email address or alternate contact details, so I can send you PDF file for review.

And I am also not able to attach PDF design file with this message.

Thanks & regards,

Mrudang

0 件の賞賛
返信

2,137件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信

2,137件の閲覧回数
mrudangshelat
Contributor IV

Thanks Yuri.

0 件の賞賛
返信

2,137件の閲覧回数
Yuri
NXP Employee
NXP Employee

I send comments via e-mail.

~Yuri.

0 件の賞賛
返信

2,137件の閲覧回数
mrudangshelat
Contributor IV

Thanks Yuri,

For your valuable feedback.

0 件の賞賛
返信