DDR3 Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR3 Configuration

跳至解决方案
1,470 次查看
vishakh
Contributor III

Hi,

I am working on a custom i.MX6 Quad processor board.

I assume there is a tool available to generate DCD values to configure DDR3.

Will someone point me where I can find this tool?

Regards,

Vishakh

标签 (1)
0 项奖励
回复
1 解答
1,254 次查看
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.freescale.com/docs/DOC-94917

Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,255 次查看
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.freescale.com/docs/DOC-94917

Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------