DDR3 Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 Configuration

Jump to solution
1,481 Views
vishakh
Contributor III

Hi,

I am working on a custom i.MX6 Quad processor board.

I assume there is a tool available to generate DCD values to configure DDR3.

Will someone point me where I can find this tool?

Regards,

Vishakh

Labels (1)
0 Kudos
Reply
1 Solution
1,265 Views
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.freescale.com/docs/DOC-94917

Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,266 Views
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.freescale.com/docs/DOC-94917

Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------