DDR3 Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,934件の閲覧回数
vishakh
Contributor III

Hi,

I am working on a custom i.MX6 Quad processor board.

I assume there is a tool available to generate DCD values to configure DDR3.

Will someone point me where I can find this tool?

Regards,

Vishakh

ラベル(1)
0 件の賞賛
返信
1 解決策
1,718件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.freescale.com/docs/DOC-94917

Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,719件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the following community thread:

https://community.freescale.com/docs/DOC-94917

Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------