DDR stress test issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR stress test issue

1,241件の閲覧回数
tony_l_cai
Contributor III

Hi,All

The following picture is the operation after DDR stress tool testing:

1.bmp

and could you tell me some possible reasons?How to solve these problems?

ラベル(2)
0 件の賞賛
返信
1 返信

1,128件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The shown  messages relate to interface between internal iROM bootloader of

i.MX6 and an application, that tries to load and run (memory) tests  via i.MX6 USB

serial boot mode. There are two possible causes of the issue.

1. The board does not start in the bootstrap (serial download) mode.

2. There is no connection between a PC and the i.MX6 board.

Please check.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信