Dear All,
I'm using the i.MX6S with eMMC and Android JB 4.3.
But the board was not booted in Low Temperature with below messages.
Could you give me any guidance for this issue?
For whole log message, refer to attached file.
** Can't read partition table on 3:0 **
booti: device don't have such partition:boot
fastboot is in init......flash target is MMC:3
** Can't read partition table on 3:0 **
Bad partition index:1 for partition:boot
** Can't read partition table on 3:0 **
Bad partition index:2 for partition:recovery
** Can't read partition table on 3:0 **
Bad partition index:5 for partition:system
wait usb cable into the connector!
Best Regards,
Eric.
Original Attachment has been moved to: eMMC_Partition.Detection.Fail.log.txt.zip
Hi Eric
I would suggest to run SDK (it has block read/write test)
and check if issue will present. Failures at low temperatures
may mean that drive strength i.MX6 and eMMC pads is too strong,
one can try to decrease it, example can be found below
https://community.freescale.com/thread/332110
also one can try other eMMC, since these chips may differ in
its driver strength characteristics.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------