DDR stress test issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR stress test issue

1,218 次查看
tony_l_cai
Contributor III

Hi,All

The following picture is the operation after DDR stress tool testing:

1.bmp

and could you tell me some possible reasons?How to solve these problems?

标签 (2)
0 项奖励
回复
1 回复

1,105 次查看
Yuri
NXP Employee
NXP Employee

  The shown  messages relate to interface between internal iROM bootloader of

i.MX6 and an application, that tries to load and run (memory) tests  via i.MX6 USB

serial boot mode. There are two possible causes of the issue.

1. The board does not start in the bootstrap (serial download) mode.

2. There is no connection between a PC and the i.MX6 board.

Please check.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复