DDR STRESS TEST, Windows Command Line?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR STRESS TEST, Windows Command Line?

2,588 次查看
jaehun718
Contributor I

I would like to use the "DDR STRESS TEST" program as the Command Line.

The product is connected by USB.


I understand that USB options are supported through the GUI.

Is there any way I can use it through Windows Command Line?

0 项奖励
回复
3 回复数

2,515 次查看
KrishnaPrasad1z
Contributor I

Hi Igor,

We too have a requirement to use DDR stress tool from command line with iMx8QXP.

Whether ddr_stress_tester_uboot_vX.xx.zip (Option 3 uboot) or similar tool available for iMx8X ?

Regards,

Krishna

0 项奖励
回复

2,515 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krishna

please look at available options on

i.MX 8/8X Family DDR Tools Release  

Best regards
igor

0 项奖励
回复

2,515 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jaehoon

available options are provided on i.MX6/7 DDR Stress Test Tool V3.00 

seems there is no command line option, probably one can consider "Option 3 U-Boot".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复