DAI SSI as capture from an external source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DAI SSI as capture from an external source

跳至解决方案
1,320 次查看
cristiansicilia
Contributor III

Dear *,

I have a schematic like this:

gpt_schematic_AUD4.png

I know that the MODEM_SSI_TXD provide the data output to a DAC, now I would like capture this data.

Is right the configuration of AUD4_TXD to MODEM_SSI_TXD?

Or the right configuration is AUD4_RXD to MODEM_SSI_TXD?

Best Regards

Cristian

标签 (3)
标记 (4)
0 项奖励
回复
1 解答
1,196 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

both options are possibel since AUDMUX can change TX and RX by bit

TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)

1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,197 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

both options are possibel since AUDMUX can change TX and RX by bit

TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)

1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复