DAI SSI as capture from an external source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DAI SSI as capture from an external source

Jump to solution
1,944 Views
cristiansicilia
Contributor III

Dear *,

I have a schematic like this:

gpt_schematic_AUD4.png

I know that the MODEM_SSI_TXD provide the data output to a DAC, now I would like capture this data.

Is right the configuration of AUD4_TXD to MODEM_SSI_TXD?

Or the right configuration is AUD4_RXD to MODEM_SSI_TXD?

Best Regards

Cristian

Labels (3)
Tags (4)
0 Kudos
Reply
1 Solution
1,820 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

both options are possibel since AUDMUX can change TX and RX by bit

TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)

1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,821 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

both options are possibel since AUDMUX can change TX and RX by bit

TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)

1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply