DAI SSI as capture from an external source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DAI SSI as capture from an external source

ソリューションへジャンプ
1,945件の閲覧回数
cristiansicilia
Contributor III

Dear *,

I have a schematic like this:

gpt_schematic_AUD4.png

I know that the MODEM_SSI_TXD provide the data output to a DAC, now I would like capture this data.

Is right the configuration of AUD4_TXD to MODEM_SSI_TXD?

Or the right configuration is AUD4_RXD to MODEM_SSI_TXD?

Best Regards

Cristian

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 解決策
1,821件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

both options are possibel since AUDMUX can change TX and RX by bit

TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)

1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,822件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

both options are possibel since AUDMUX can change TX and RX by bit

TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)

1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信