Creating bootable SD for Linux on iMX28 EVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating bootable SD for Linux on iMX28 EVM

4,163 Views
dennisg
Contributor I

I am running the mk_mx28_sd as described in 5.1.3.1 of the users guide. I am able to determine my SD card is /dev/sdb via the method described. However after removing the card as instructed and running ./mk_mx28_sd /dev/sdb it does nothing (no prompting) and just returns immediately to the shell prompt.

I think I am missing something obvious but at a loss to see it right now. Any pointers would be appreciated.

 

TIA

Tags (1)
0 Kudos
Reply
6 Replies

3,627 Views
RogerioNunes
NXP Employee
NXP Employee

Hi Matt,

 

One more thing that helps is to support mmcblk.

I've fixed the script you shared to support this kind of device as well.

Pls find attached the new file.

 

Regards.

Rogerio Nunes.


Matt Clemens said:

The version in the attached should work. We're working on getting this updated on the main MX28 pages on freescale.com.
0 Kudos
Reply

3,627 Views
dennisg
Contributor I
I prefer chmod 755 ;-)
0 Kudos
Reply

3,627 Views
iMxGuy
Contributor II
chmod +x mk_mx28_sd
0 Kudos
Reply

3,627 Views
dennisg
Contributor I

Thanks much !



Matt Clemens said:

The version in the attached should work. We're working on getting this updated on the main MX28 pages on freescale.com.
0 Kudos
Reply

3,626 Views
mdc
Contributor V
The version in the attached should work. We're working on getting this updated on the main MX28 pages on freescale.com.
0 Kudos
Reply

3,626 Views
daiane_angolini
NXP Employee
NXP Employee
0 Kudos
Reply