Creating bootable SD for Linux on iMX28 EVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating bootable SD for Linux on iMX28 EVM

4,361件の閲覧回数
dennisg
Contributor I

I am running the mk_mx28_sd as described in 5.1.3.1 of the users guide. I am able to determine my SD card is /dev/sdb via the method described. However after removing the card as instructed and running ./mk_mx28_sd /dev/sdb it does nothing (no prompting) and just returns immediately to the shell prompt.

I think I am missing something obvious but at a loss to see it right now. Any pointers would be appreciated.

 

TIA

タグ(1)
0 件の賞賛
返信
6 返答(返信)

3,825件の閲覧回数
RogerioNunes
NXP Employee
NXP Employee

Hi Matt,

 

One more thing that helps is to support mmcblk.

I've fixed the script you shared to support this kind of device as well.

Pls find attached the new file.

 

Regards.

Rogerio Nunes.


Matt Clemens said:

The version in the attached should work. We're working on getting this updated on the main MX28 pages on freescale.com.
0 件の賞賛
返信

3,825件の閲覧回数
dennisg
Contributor I
I prefer chmod 755 ;-)
0 件の賞賛
返信

3,825件の閲覧回数
iMxGuy
Contributor II
chmod +x mk_mx28_sd
0 件の賞賛
返信

3,825件の閲覧回数
dennisg
Contributor I

Thanks much !



Matt Clemens said:

The version in the attached should work. We're working on getting this updated on the main MX28 pages on freescale.com.
0 件の賞賛
返信

3,824件の閲覧回数
mdc
Contributor V
The version in the attached should work. We're working on getting this updated on the main MX28 pages on freescale.com.
0 件の賞賛
返信

3,824件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee
0 件の賞賛
返信