Create an image with torch 2.0 or above

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create an image with torch 2.0 or above

1,840 Views
Sho_1
Contributor I

Hi,

 

I need to create an image with torch 2.0 or above, using the demo in nxp-github I can  create image with torch 1.9.1post2 using Yocto Project BSP 6.1.1_1.0.0 Release. 

Can I change line:9 in python_git.bb file such that torch 2.0 will be install? or I must do it in other way? How?

Appreciate any help, 

# IMX8M

IMX8MPLUS 

0 Kudos
Reply
5 Replies

1,645 Views
Sho_1
Contributor I

Hi @Harvey021 ,

Is there a new release date?

 

Best regards,

Sho

 

0 Kudos
Reply

1,797 Views
Sho_1
Contributor I

Hi @Harvey021

Thanks for your response.

Is there a release date?

 

Best regards,

Sho

0 Kudos
Reply

1,788 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

As I know, will be Q2.

 

Best regards

Harvey

0 Kudos
Reply

1,822 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Sho_1 

The current release commit (SRCREV = "ef997d8f79877295e69e5cf34b524eea603c1fae") does not support for the 2.0 or above. Next release might support it.

 

Best regards

Harvey

0 Kudos
Reply

1,650 Views
Sho_1
Contributor I
Hi,

Is there a new release date?


Best regards,

Sho


0 Kudos
Reply