Create an image with torch 2.0 or above

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create an image with torch 2.0 or above

1,834件の閲覧回数
Sho_1
Contributor I

Hi,

 

I need to create an image with torch 2.0 or above, using the demo in nxp-github I can  create image with torch 1.9.1post2 using Yocto Project BSP 6.1.1_1.0.0 Release. 

Can I change line:9 in python_git.bb file such that torch 2.0 will be install? or I must do it in other way? How?

Appreciate any help, 

# IMX8M

IMX8MPLUS 

0 件の賞賛
返信
5 返答(返信)

1,639件の閲覧回数
Sho_1
Contributor I

Hi @Harvey021 ,

Is there a new release date?

 

Best regards,

Sho

 

0 件の賞賛
返信

1,791件の閲覧回数
Sho_1
Contributor I

Hi @Harvey021

Thanks for your response.

Is there a release date?

 

Best regards,

Sho

0 件の賞賛
返信

1,782件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

As I know, will be Q2.

 

Best regards

Harvey

0 件の賞賛
返信

1,816件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Sho_1 

The current release commit (SRCREV = "ef997d8f79877295e69e5cf34b524eea603c1fae") does not support for the 2.0 or above. Next release might support it.

 

Best regards

Harvey

0 件の賞賛
返信

1,644件の閲覧回数
Sho_1
Contributor I
Hi,

Is there a new release date?


Best regards,

Sho


0 件の賞賛
返信