Correct IMX8 processor reference manual?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Correct IMX8 processor reference manual?

7,105 Views
jcole1
Contributor I

I have downloaded the IMX8 processor reference manual in order to access some of the GPIO registers in a device driver.

The document I used was this one:

https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf 

According to the above, the GPIO registers are in the region of 0x5D080000, however attempting to access them causes GPFs.

I consulted a manual for the IMX7 where the registers are in the region of 0x30200000 and they appear to work.


The CPU is on a SOM made by Compulab; the cl-som-imx8

The cpuinfo on the target displays 4 processors:

# cat /proc/cpuinfo
processor : 0
BogoMIPS : 16.66
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

Are there variations amongst the IMX8 family or is there a different reference manual available?

0 Kudos
Reply
10 Replies

6,676 Views
jcole1
Contributor I

Wow.  I am astonished and dismayed.

It may be a third party board, but it is using your CPU (iMX8MM)

Perhaps you could take a leaf from the TI forum where they would answer questions on their products irrespective of how they are deployed.

0 Kudos
Reply

6,676 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jason,

So sorry that my reply make you dismayed. Here I mean the software and board information you can contact the third company, because the hardware and software are design by them they will give more effective and fast reply. I see your above information, one image is work well, another not, so the hardware is OK.  About the chip questions you can contact us.

Have an nice day

Best Regards

Rita

0 Kudos
Reply

6,674 Views
jcole1
Contributor I

It's possible that this issue could be DTS-related; I have one kernel image where this issue occurs, on another it does not.

0 Kudos
Reply

6,674 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jason,

I see that you are using the third company board, so about the software and board information you can contact their supportWelcome to CompuLab Support | CompuLab .

Have a nice day

Rita

0 Kudos
Reply

6,674 Views
jcole1
Contributor I
0 Kudos
Reply

6,674 Views
jcole1
Contributor I

I am also experiencing difficulty accessing the I2C registers (0x30A20000 etc).  I use the same mechanism as I do for accessing the GPIO and IOMUX registers, and they all work
e.g:


define I2C3_CR   0x30A40008

static void __iomem *vpIMX8_I2C3_CR;

vpIMX8_I2C3_CR = devm_ioremap(thisDev, I2C3_CR, sizeof(u16));

readVal = ioread16 (vpIMX8_I2C3_CR);      //system hangs here......

Is there anything I am doing wrong here?

0 Kudos
Reply

6,674 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which product are you using?

0 Kudos
Reply

6,674 Views
jcole1
Contributor I

I see - I have found this one for the iMX8MM, which is very different to the DQ/XP:

https://cache.nxp.com/secured/assets/documents/en/reference-manual/IMX8MMRM.pdf 

Are there any others?

Jase

0 Kudos
Reply

6,674 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, the i.MX8DQ/XP is different with the i.MX8MM. They are different products.

0 Kudos
Reply

6,674 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Different products have they own RM, all the i.MX8 series products are here. The i.MX8&i.MX8X are still on PRE-PRODUCTION.

0 Kudos
Reply