What value resistor should pull WDOG_B high?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What value resistor should pull WDOG_B high?

ソリューションへジャンプ
2,625件の閲覧回数
adevries
Contributor V

Hello,

In the i.MX 8M Mini hardware developer's guide, table 8, it suggest to pull GPIO1_IO02 (WDOG_B, ball AG13) high with a 100k ohm pull-up resistor. However, in section 5.5 of the same document, Note 2 says to pull the pin high with a 4.7k ohm resistor. Which value is actually recommended?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,486件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi adevries 

100k ohm is sufficient, also one can use internal pull-up as described in

attached i.MX8M Mini EVK schematic p.12.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,487件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi adevries 

100k ohm is sufficient, also one can use internal pull-up as described in

attached i.MX8M Mini EVK schematic p.12.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------