Copy entire folder structure using Mfgtool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Copy entire folder structure using Mfgtool

ソリューションへジャンプ
2,679件の閲覧回数
stephenhewitson
Contributor III

Hi,

We use mfgtool to push a WinCE image ("nk.nb0") to an iMX28. As part of this process I also want to send the application we will be running.

Currently we are required to plug a USB stick containing the application into the product and copy the *.cab file across manually, followed by unpacking the application.

I've seen that it might be possible to call <CMD type="push" body="mkdir /test"/> to create a folder, but is it possible to define a file (or entire unpacked folder structure) that is copied across by mfgtool?

Thanks,

EDIT:

Ok, so I can send individual files using

<CMD type="push" body="filename:NANDFlash\\sandy.mp3">Specify the file name and path in the board.</CMD>

<CMD type="push" body="send" file="files/sandy.mp3">Sending a file from the host.</CMD>

I'd still be interested if an entire folder structure (subfolders and files) was possible, without having to send each file separately.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,460件の閲覧回数
stephenhewitson
Contributor III

Apparently the write command in the WinCE (nk.nb0) does not support full folder directory, and the only way of fixing this is to modify the image to allow it.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,460件の閲覧回数
stephenhewitson
Contributor III

Ok, so I can definitely push a file across, but I've not managed to create a subfolder yet.

Has anyone managed to do this, or at least could point me in the right direction?

0 件の賞賛
返信
2,461件の閲覧回数
stephenhewitson
Contributor III

Apparently the write command in the WinCE (nk.nb0) does not support full folder directory, and the only way of fixing this is to modify the image to allow it.

0 件の賞賛
返信