About MAC status signal of ENET of i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MAC status signal of ENET of i.MX6

ソリューションへジャンプ
1,355件の閲覧回数
yuuki
Senior Contributor II

Dear All,

I refer to the following part of a reference manual.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
- Table 23-130. Receive FIFO thresholds definition(P.1189)

"MAC status signal" is described here.
However, I cannot find explanation about this MAC status signal.

What does this signal show concretely?

Best Regards,
Yuuki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,262件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The MAC status signal is internal one of ENET module.
For programming please use status bits, available in Interrupt
Event Register (ENET_EIR).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,263件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The MAC status signal is internal one of ENET module.
For programming please use status bits, available in Interrupt
Event Register (ENET_EIR).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信