Console UART port changing in imx linux branch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Console UART port changing in imx linux branch

Jump to solution
3,228 Views
vivekrajpara
Contributor III

Hi All,

I am working with imx7s and free scale linux git repository.

I need to change console UART port of the Cortex A7 core so that I can access U-Boot prompt and Kernel Logs on different UART.

Currently logs are transferred to UART 1 port I need to transfer them to UART 4 port.

Can anyone suggest required changes for this?

Thanks,

Vivek

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vivek

one can look at Sabre AI example where uart4 is used, so in

uboot/include/configs/mx6qsabreauto.h :

#define CONFIG_MXC_UART_BASE    UART4_BASE
#define CONFIG_CONSOLE_DEV        "ttymxc3"

with kernel boot parameter console=ttymxc3,115200

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
2,423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vivek

one can look at Sabre AI example where uart4 is used, so in

uboot/include/configs/mx6qsabreauto.h :

#define CONFIG_MXC_UART_BASE    UART4_BASE
#define CONFIG_CONSOLE_DEV        "ttymxc3"

with kernel boot parameter console=ttymxc3,115200

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,422 Views
rootb3r
Contributor II

I'm facing the same issue on imx28evk custom board for Wink Hub 1 but the uboot/include/configs/mx28evk.h file doesn't seem to have the CONFIG_MXC_UART_BASE & CONFIG_CONSOLE_DEV config.

Waiting for reply.

0 Kudos
Reply
2,422 Views
vivekrajpara
Contributor III

Thank you Igor,

These settings worked. I just need to do extra iomux settings in U-Boot code in addition to steps mentioned by you

Best Regards,

Vivek

0 Kudos
Reply