Configuration of LPDDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuration of LPDDR

1,998件の閲覧回数
Vivekdutt
Contributor I

Hi,

NXP,

  I'm using i.MX8M Mini EVK board which is very new for me. I want to know which are the things required to change the SIZE of the LPDDR4. And how to configure the LPDDR. Below the tool i'm using.

1. I'm using DDR_MSCALE_tool_V_3.20

2. RPA for register configuration V18.

But i want to change the RAM from 2GB to 1GB.

I want to know to generate the .ds file.

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,992件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vivek

 

for different memory size recommended to run DDR Test (and use RPA tool) on below

link and change image as described in document: MSCALE_DDR_Tool_User_Guide

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

also use #define PHYS_SDRAM_SIZE in  uboot-imx/tree/include/configs/imx8mm_evk.h

https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8mm_evk.h?h=imx_v2020.0...

 

Best regards
igor

0 件の賞賛
返信